Export a FactoryTalk Optix Application
Export a FactoryTalk Optix Application to deploy the application to client devices that are not accessible in the network.
-
Select the arrow next to
Save to open the drop-down menu and then select .
-
In the dialog, complete:
-
Platform. Select the operating system of the client device.
-
Location. Type the path to the location where you want to save the FactoryTalk Optix Application. Alternatively, select the folder icon to browse to the folder.
Tip: A folder can only contain one FactoryTalk Optix Application. Each FactoryTalk Optix Application must use a separate folder.
-
-
(optional) If available, fill Password to password-protect the exported application.
The exported application is encrypted. You will be prompted to enter the password when importing the application to the client device.
- Select Export.
A progress window displays while the FactoryTalk Optix Application is being exported. After the export has completed, a dialog appears to inform you that the FactoryTalk Optix Application was successfully exported to the location specified.