Create variables
Create a variable that mimics raw data received from a controller and an analog variable that presents the controller data as a temperature unit.
-
Create a variable that mimics raw data received from a controller:
- In Project view, right-click Model and select .
-
Hover-over the variable, select
, and enter FromPLC.
- In Properties, set the FromPLC (Int32) property value to 60.
-
Create an analog variable that presents the controller data as a temperature unit: