Create a label
Create a label that displays temperature in a format adjusted to the locale of a logged-in user.
-
Create the label:
- In Project view, right-click MainWindow (type) and select .
-
Hover-over the label, select
, and enter TemperatureLabel.
-
Create a label variable:
-
Create a complex dynamic link between Text and AnalogVariable1 with the use of a string formatter:
- StringFormatter1
- {0} {1}
- {0} DynamicLink
- {1} DynamicLink
For more information about dynamic links, see Create dynamic links.