Develop a motor management dashboard
The UI contains a list of motors and gauges that display speed and acceleration values.
Prerequisites
To develop the project
- Create Motor objects.
- Create a list of motors.
- Create a motor values widget (type).
- Create a speed gauge and labels.
- Create an acceleration gauge and labels.
- Create a motor values widget instance.
- Arrange the interface elements.
- Save the project.

Select Run to run the project using the client emulator to test your project. To run the project on a remote client, see Add a client device.