Create a motor values widget instance
Create a motor values widget instance from the motor values widget type.
- In Project view, right-click MainWindow (type) and select .
-
In Properties, create a dynamic link between Motor and .
For more information about dynamic links, see Create dynamic links.