Develop a temperature change alarm
Develop an alarm that signals when temperature exceeds a set value.
Prerequisites
To develop the project
- Create a temperature alarm.
- Create a thermometer linear gauge.
- Create an alarm grid.
- Arrange the interface elements.
- Save the project.
Select Run to run the project using the client emulator to test your project. To run the project on a remote client, see Add a client device.