Edit a NetLogic
Modify the NetLogic code by using an external code editor.
Prerequisites
Set the default external code editor. See Set the default code editor.
To edit a NetLogic
-
In Project view, double-click a NetLogic object.
The default external code editor opens.Tip: Rockwell Automation recommends using Microsoft Visual Studio 2022 or Microsoft Visual Studio Code as the default code editor. Some development assistance features may not be available when using a different code editor.
-
In the external code editor, edit the NetLogic code and save the file.
Tip:You can expose custom methods by adding such declarations:
[ExportMethod] public void MyCustomMethod1() { //Add custom code here }