Create an OPC UA method callable by an external OPC UA Client
reate an OPC UA method callable by an external OPC UA client and then edit its code in an external code editor.
Prerequisites
Set the default external code editor. See Set the default code editor.
To create an OPC UA method callable by an external OPC UA Client
- Create an object type. See Create an object type.
- In the Project view pane, right-click the object type and select Add custom behavior.
-
Right-click the object type and select Edit with .NET code editor (external).
The external code editor opens. The following code is added in the NetLogic:
[CustomBehavior] public class testTypeBehavior : BaseNetBehavior { public override void Start() { // Insert code to be executed when the user-defined behavior is started } public override void Stop() { // Insert code to be executed when the user-defined behavior is stopped } #region Auto-generated code, do not edit! protected new testType Node => (testType)base.Node; #endregion }
In the code editor, develop the method.