Cancel a task
A task can be canceled at runtime. You cannot run a canceled task.
Making a task cancelable
You can cancel a task if the value returned from reading its IsCancellationRequested property is appropriately managed in the method that executes, usually using conditional instructions.
The
IsCancellationRequested property can have the following values:
false- Cancellation not requested.
true- Cancellation requested.
To use the property within the method, indicate the task as the argument of the same method, specifying its type.
In the following example,
myTask is a task and ProcessCsvFile() is the method that executes:
private void ProcessCsvFile(LongRunningTask myTask)
{
// Code to execute
}
For a complete example, see Constructor: LongRunningTask(action, executingNode).
Cancel a task
You cancel a task by invoking the
Cancel() method on the task. See the following example.
myTask.Cancel();
The method sets the value of the task IsCancellationRequested property to True.