Collections
A collection is a C# object that contains multiple objects. You can use collections for counting, iterating, adding, and removing child nodes of a given node.
Generic children collections
Available in every IUANode C# object and each project node. Generic children collect the object/node properties and other objects/nodes that are its direct children.
Specialized collections
|
Type of project object |
|
Collection |
Type of collection object |
|---|---|---|---|
|
Data logger |
|
|
|
|
Event logger |
|
|
|
|
OPC UA Client |
|
|
|
|
OPC UA Server |
|
|
|
|
|
|
||
|
|
|
||
|
Report |
|
|
|
|
Retentivity database |
|
|
|
|
Store |
|
|
|
|
Table |
|
|
|
|
Circular gauge |
|
|
|
|
Linear gauge |
|
|
|
|
Data grid |
|
|
|
|
Navigation panel |
|
|
|
|
Trend pen |
|
|
|
|
XY chart line |
|
|
|
|
Communication station |
|
|
|
|
|
|
||
|
Containers Graphical objects that can have children |
- |
|
|
|
Object |
|
|
BaseObject
Tip: Instances of any derived types that are not represented in
InstanceNodeCollection. They can be listed manually with the derived types first. |
|
Variable |
|
|
BaseVariable
Tip: Instances of any derived types that are not represented in
InstanceNodeCollection. They can be listed manually with the derived types first. |