Configure a REST API Client
Add a REST API Client NetLogic from Libraries to expose HTTP methods.
-
From the toolbar, select
Template Libraries.
- In Libraries, search for REST API Client.
-
Under Components, drag REST API Client onto NetLogic in Project view.
In Project view, RESTApiClient appears in the NetLogic folder.
- Close Libraries.
-
(optional) In Properties edit:
-
Timeout. Time after the request is canceled if no response is received. Defaults to ten seconds.
-
UserAgent. String that represents the application from which the request originates. Defaults to FTOptix.
-
Use the exposed GET, POST, and PUT methods in your application logic. See HTTP methods.
Tip: For example, you can trigger the methods with a MouseClick event of a Button object.